Power SCADA Anywhere

Power SCADA Anywhere is an HTML5 streaming application that allows for the visualization of the Power Operation Runtime from any HTML5 compliant browser (Edge, Chrome, Firefox, etc) by streaming a remote desktop application from a Client Access. This is a legacy solution that is being substituted with the new HTML5 PO 2021 web client.

Use the links in the following table to find the content you are looking for:

Topic Content
Power SCADA Anywhere component A description of the Power SCADA Anywhere component, including purpose, what's new, upgrade considerations, supported operating systems, host requirements, browser requirements, licensing options, and design considerations.
Power SCADA Anywhere architectures Example Power SCADA Anywhere architectures.
Web Client versus Thick Client A comparison of features available in the thick client (Power SCADA Anywhere) and the HTML5 web client.